AXIS#.MOTOR.TBRAKETO

Description

When a drive is disabled (due to user command, digital input, or fault), the brake will normally not be applied until velocity has fallen below AXIS#.ZEROV. In some instances, such as a vertical axis, it may be desirable to apply the brake regardless of velocity.

AXIS#.MOTOR.TBRAKETO sets the maximum time allowed to pass between drive disable and application of the motor brake. After this time, the brake will be applied even if velocity is higher than AXIS#.ZEROV.

To disable the timer, set the value to -1 (default).

Context

For more information see Brake and Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Milliseconds

Range

-1 to 30,000

Default Value

-1 (function disabled)

Data Type

Integer

See Also

AXIS#.ZEROT, AXIS#.ZEROV, AXIS#.DISTO
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
AXIS1.MOTOR.TBRAKETO

500bh

1ch

Signed32

-

-

Read/Write

No

AXIS2.MOTOR.TBRAKETO

510bh

1ch

Signed32

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MOTOR.TBRAKETO

6223

184F

Signed32

Read/Write

-

AXIS2.MOTOR.TBRAKETO

71759

1184

Signed32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.TBRAKETO

6223

Signed32

Read/Write

-